This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

configuration of CDCM6208V1

我对CDCM6208v1的配置如下:初次级参考输入时钟为10MHz单端时钟,在pin mode 下,输出时钟正常,配置为SPI模式后,对register 0 到 20的配置如下:(以下为16进制数)01B9,0024,003D,08F0,0097,0001,0000,0001,0000,1C53,0090,0000,1E53,00B6,6666,1C53,03D0,0000,0001,0000,0000,读了写入的寄存器的值,发现写入的值正常写入,但是读register21和register40的值分别为0007,0102,register 21显示的是PLL失锁,两个输入无参考,实际上我的输入10M是一直都有的。在pin模式下,时钟都可以正常输出。我想要的输出是Y4=62MHz,Y5=50MHz,Y6=10MHz,LVCMOS输出。但在SPI模式下一个输出都没有,求帮忙!