This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about X-MODE and long distant transmission of SN65DP159

Other Parts Discussed in Thread: SN65DP159

hi,everyone,

In my project, I use SN65DP159 and Xilinx FPGA XC7K410T to design a 4K2K/60Hz monitor with DisplayPort interface. SN65DP159 works in a special mode called X-Mode according to TI's application document <<SLLA358>>, and my hardware design is complied with this document. the monitor can works normally with a DP cable which is less than 2 meters connected to a PC. but if I change to a 5-meters cable, the monitor has no display output. The new cable is tested OK when connect a PC to a samsung 4K2K monitor. So it looks like the SN65DP159 does not work. the attachment is the source code for SN65DP159 including dp159.h, dp159.c, main.h, main.c. I want to know whether the configuration for SN65DP159 is correct or not? How to modify the configuration about SN65DP159 to satisfy long distance signal transmission?

thanks.

src.rar