This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI技术大牛们,请教一个940问题:Ds90UB925串行器+DS90UB940解串,925的输入是DVP camera,通过940转出来的MIPI信号波形异常,见附件,是否940寄存器设置不当导致?
这是哪个pin脚的波形?后面接了什么吗?
用925的“Internal Pattern Generation”试试。
Hi Jex,
CSI时钟波形这样时,屏幕显示正常吗?940的PASS和LOCK信号是否正常?
用925产生HD 1080p30 试试,这套参数跟你的比较接近。
CSI2设置可以看下检查下寄存器0x6b。
Hi Jason,
CSI时钟波形这样时,屏幕显示正常吗?=>不正常,没有图像。屏幕是黑的。
940的PASS和LOCK信号是否正常?=》正常,都是高电平
用925产生HD 1080p30 试试,=》试过了,925的1080p30 RAW10波形正常,图像OK
CSI2设置可以看下检查下寄存器0x6b。=》0x6b寄存器之前就设置过了0x7c值,波形就是有问题的这个。能否帮忙提供 CSI-2 indirect register的所有寄存器,940的spec中只有 0x9,0x13,0x14,0x16,0x2E。附件的波形把 每行(Line)的数据分成了两次来发送,个人认为是 MIPI寄存器设置不够详细,默认可能是个比较小的分辨率,比如840*480,而我们的是1920*1080,所以才被分成了两次来发送的。