按照网友的这个寄存器进行配置,前一个数值为寄存器地址,后一个数值为写入值,不过配置完发现不是网友说的PLL为200.45M,而是100M。
我按照我项目的需要进行配置PQRN四个值后,发现最高PLL也是100M,是不是我们哪个寄存器的写入值是不对的呢?请大家鉴定下
2,0xb4, //2 10110100
3,0x01, //3 0x01
4,0x02, //4 00000010
5,0x28, //5 00101000
6,0x40, //6 0x40
0x14,0x6d, //14 01101101
0x15,0x02, //15 00000010
0x16,0x06, //16 0 0x06 //P2div=6
0x17,0x07, //17 0 0x07 //P3div=7
0x18,0x00, //18 0x00 //PLL状态0不用,写缺省值
0x19,0x40, //19 0x40
0x1a,0x02, //1a 0x02
0x1b,0x08, //1b 0x08
0x1c,0xbc, //1c 0xbc //PLL状态1,写NRQP值 N"=0xbc7,R=0x45,Q=0x1d,P=2,
0x1d,0x72, //1d 0x72 //将这4个数按二进制位排好,后面在加两位构成32位4个字节。
0x1e,0x2b, //1e 0x2b
0x1f,0xab, //1f 0xab //PLL输出范围>175MHz, 1f最后2位=11b