我现在使用的CPU为5V系统,RAM和FLASH是3.3V,SPI口,时钟芯片是3.3V,I2C接口,是否可以使用一片TXS0108或TXB0108?另外我看TXS0108的低电平输入最大值VIL是0.15V,对接到这个系统中有问题吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你只要满足A端口和B端口可接受高低电平要求即可,请看数据手册:http://www.ti.com.cn/product/cn/TXS0108E?keyMatch=TXS0108&tisearch=Search-CN-Everything
可以使用,建议使用TXS系列,TXBxx的不适用于I2C这种开漏架构的应用。
另外还要注意SPI的频率是否能够支持,TXS最大能够支持110Mbps的速率。
请问下我用TXS0108E把A/B端的电平接反了,A大于B了。这样还能用的吗?谢谢!
手册6.3 Recommended Operating Conditions有相关参数,您可以看看。至于您说的接反了具体什么意思我还不太清楚。
我说的接反是,正常是A<=B,但是,我接成A>=B.这样芯片是否还可以正常工作。我在手册上看到的是,接反的是会引起把芯片损坏,并,没有说不能工作。请帮忙指教下。谢谢!
满足VCCA VCCB工作电压范围,则芯片不会被烧坏。
电压满足的,我想问的是在A端电压高于B端电压的情况下,那这个芯片还能正常工作的吗?谢谢!
A端电压大于B端电压的话就不能保证正常工作了。
必须满足VCCA<=VCCB.