This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7221A为什么静态电流这么大?

Other Parts Discussed in Thread: ISO7221A

由于项目中一直在使用ADuM1201,现在ADI的料比较缺货,所以打算用ISO7221来替代,结果拿到样品之后测试发现ISO7221的静态电流大的让人崩溃,一开始以为是电路设计错误,后来仔细看一下文档才知道确实如此,看一下下图的对比就可以知道ISO7221根本就是个失败的产品,完全不是一个数量级的

这个是ISO7221的静态电流

这个是ADuM1201的静态电流

  • 也不能说是失败,只是针对不同的应用。如果你特别关注低功耗可以选择ISP7321

  • 你说的这颗料查不到啊,是TI的吗?能否给个链接?

  • jeffrey Qe 说:

    你说的这颗料查不到啊,是TI的吗?能否给个链接?

    ISO7221是TI的。ADUM1201是ADI的。

    http://www.ti.com/product/ISO7221A/technicaldocuments

  • 厂家不同这个我自然知道,只是楼上的说的颗料应该是型号写错了,我查到应该是ISO7321 不是ISP7321,ADuM1201的功耗基本和ISO7321(主打低功耗)一样了,但是价格方面还是ADI的占很大的优势,现在市面上的隔离相关产品都是使用ADI的这颗料,问题是我想不明白,为什么TI的这颗7221功耗那么大?本来这种低压隔离产品对功耗就比较敏感,因为低压小功率的隔离电源无论在效率或者体积上都要求比较苛刻,所以我觉得TI简直是破罐破摔的节奏,这么大的静态电流,我特么用分立元器件也能做出来啊。

  • 厂家不同这个我自然知道,只是楼上的说的颗料应该是型号写错了,我查到应该是ISO7321 不是ISP7321,ADuM1201的功耗基本和ISO7321(主打低功耗)一样了,但是价格方面还是ADI的占很大的优势,现在市面上的隔离相关产品都是使用ADI的这颗料,问题是我想不明白,为什么TI的这颗7221功耗那么大?本来这种低压隔离产品对功耗就比较敏感,因为低压小功率的隔离电源无论在效率或者体积上都要求比较苛刻,所以我觉得TI简直是破罐破摔的节奏,这么大的静态电流,我特么用分立元器件也能做出来啊。