This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LMC555定时器datasheet上面的疑问

Other Parts Discussed in Thread: LMC555

最近在选一个定时IC,看到LMC555有触发功能,想用它设计一个PWM波触发,PWM波输出但是占空比可调的电路。

看了datasheet之后有这么一个疑问。上面写的Measure Delay from Trigger to Output时间tpd是100ns,但是Figure5里面又出现了一个Time Delay表格,和设置的R/C值有关,最小的TIME DELAY都有10us,那么这个从触发到输出的延时到底有多少呢?

  • Hi Steven

    你把两个概念弄混淆了。

    100ns是触发信号触发成功到输出信号的延迟。

    Figure5中是触发后输出信号保持高的时间长度,该时间=1.1*RA*C, 图中的RC计算结果和该公式相符。

    10us是触发信号恢复到高状态后的时间和输出信号回复到低之前的一个最短时间要求,规格书中这个句子有点拗口,你多读理解下。

  • 多谢回复,您的回复是正确的,我设计了一个TIME DELAY,也就是Th为5us的PWM波输出,结果发现输出PWM波高电平持续时间有5ms那么多。

    所以LMC555是不适合输出很高频率的PWM波的。

    那么问题来了,如果我想用一个占空比50%频率为200kHz的PWM波去触发,输出一个占空比为35%频率为200kHz的PWM波,有没有什么样的IC可以实现这个功能呢?

  • 坛友你所说的的确是正解