This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI工程师们,你们好!
最近设计继电器驱动电路,使用ULN2803来控制继电器,现在的问题主要是:继电器要求输入驱动电压为5V,但是ULN2083的导通压降为0.9V—1.7V左右,导致继电器两端电压为4V,继电器驱动能力不够,而且这种继电器用在特殊领域,不能更换。
本来打算从两个方面来解决这个问题(1)、提高继电器供电电压,通过12V转6V或者7V稳压芯片,这种芯片需要输出电流不低于500mA ,查了很多都是buck型的,很少有LDO型的,buck型的输出纹波比较大,请问对继电器是否有影响,TI的工程师你们能否推荐一款这种芯片。
第二个解决方案就是,选用低导通压降管子,再TI的官网上找了两款芯片外围驱动芯片一个是SN75477,另一个是TPL7407L导通压降比较小,导通压降在0.2V左右,这里想请问一下SN75477和TPL7407L是否可以驱动继电器,设计过程中是否有一些注意事项。
最后就是想问一下是否还有其他解决达灵顿管导通压降的可实现方法,谢谢了!
你好,
(1)Buck电路的输出纹波对继电器有影响,但影响不大,可以增大输出电感或增大buck电路的开关频率或增大输出电容,都可以降低buck的输出纹波,推荐的芯片如:TPS54335
(2)SN75477的输出电流为300mA,达不到所述的要求;TPL7407L的datasheet中的曲线图可以看到在输出电流为500mA时的压降为1V左右,而ULN2803为1.4V左右,可以说TPL7404L在压降上略有优势,但可能仍然解决不了根本问题。
其他的方法可以试一试将ULN2803的两个输出端并联在一起,降低每路的输出电流,从而降低导通压降。