This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UR905对接DS90UR910

TI工程师,你好!
我是公司正在调试DS90UR905连接DS90UR910 方案,
目前情况是这样的,两个ic都可以正常工作,I2C读取正常,BIST模式下,也测试通过 了,PASS高,lock高。
但在normal模式下,DS90UR905有信号输出,但DS90UR910 端,lock时高时低,不稳定,DS90UR910 的csi-2输出也没有信息。

请问,有什么好的解决思路吗?,请指导一下,谢谢!

直接通信,DS90UR905或DS90UR910 需要通过I2C配制什么吗?
  • 你好,yinnian

    在BIST模式下pass一直为高,说明芯片在这个像素时钟下,UR905到UR910这个子系统是没有问题的。但是换到你的正常应用中,像素时钟改变了,输入的时钟信号质量也变化了,这将导致串行后的高速信号速率改变,pcb走线和线缆在不同速率下的高频衰减是不一样的。

    基于以上分析,建议如下

    1. 示波器看看输入R905的信号质量如何,量化分析是,使用差分探头测量UR905输出的高速信号的眼图中的jitter,是否和规格书中所列比较靠近输入时钟的数值接近, 7.11中的tDJIT。

    2. 通过寄存器或者管脚修改UR910中EQ的数值,看看lock是否稳定。