Other Parts Discussed in Thread: SN65HVD251
您好,我在查看CAN收发器的手册时注意到,5V供电的CAN收发器,器件功耗基本在100mw左右(比如SN65HVD251),但是其显性输出时供电电流ICC最大可以达到65ma,这个值是怎么计算出来的?我在设计低功耗系统时,CAN部分的功耗该怎么计算?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN65HVD251
您好,我在查看CAN收发器的手册时注意到,5V供电的CAN收发器,器件功耗基本在100mw左右(比如SN65HVD251),但是其显性输出时供电电流ICC最大可以达到65ma,这个值是怎么计算出来的?我在设计低功耗系统时,CAN部分的功耗该怎么计算?
65mA的测试条件是:D at 0 V, 60-Ω load, Rs at 0 V时测得的通过VCC的电流大小。
100mW的功耗也是有测试条件的,在数据手册上一般都给出测试条件。
你指的设计低功耗,是指的将SN65HVD251进入standby模式,需要将Rs pin拉高,此时流经VCC的电流只有uA级,静态功耗为Vcc*Icc。
通常情况下我们会在CANH和CANL中间接上120欧姆的电阻,那这个时候在D at 0 V,Rs at 0 V时VCC的电流大概是什么值?比65ma大还是小?
这里的65mA应该指的是driver在显性时的最大Icc电流。