This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.使用Soft Pin Programming Mode (HW_SW_CTRL = 0)模式配置125MHZ时钟没有成功;
2.改用Hard Pin Mode(HW_SW_CTRL = 0)模式,ROM-0(GPIO[5:0]=0),8路时钟输出25MHZ,全部有输出;改成ROM-1,8路时钟输出只有OUT2-3的25MHZ有输出,Codeloader读取发现已经配置成功,但是示波器测量除了OUT2-3的25MHZ有输出,其他几路都没有。
原理图配置如下:
1.参考时钟25Mhz;
2.REFSEL拉高;
请TI员工大神帮忙看下问题;
你好!
按照你的描述,如果8个口都是出25M,那应该是HW_SW_CTRL = 1, 而不是0,请你确认下
如果HW_SW_CTRL = 1,ROM-1,你的codeloader界面读取是正常的。
1. 建议你在register里面检查下寄存器的状态,看是否有问题。
2. 用coderloader更改几个通道的状态,看LMK03328能否正常响应,比如更改到和OUT2,OUT3一样的配置
3. 你的输出是LVPECL的,但是从你的原理图上并没有看出是LVPECL的相应电路,请你再确认下