你好,LMX2571支持4种调制模式,其中SPI和fast SPI两种模式的接口怎么接,使用MICROWIRE还是FSK_D[0:2]/FSK_DV,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SPI和fast SPI都是采用MICROWIRE。 FSK PIN mode采用FSK_D[0:2]/FSK_DV。
FSK_D[0:2]/FSK_DV用在FSK PIN mode和FSK I2S mode,如果使用SPI或者Fast SPI模式的话,可以将FSK_D[0:2]/FSK_DV悬空。通过配置register 34的[bit 1:0] FSK_MODE_SEL0来选择四种模式中的一种。