This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913Q调试问题(急!!!)

1.我司正在做个摄像头LVDS传输,后端DS90UB914Q是在客户的主板上,目前我司调试的时候遇到一个问题:913+摄像头板子刚开始接入客户提供的设备上电时,测试913的电压1.8V正常,外部晶振24M正常输入913有波形, 经过913分频没有12M时钟输出(913采用外部晶振模式),摄像头无法工作,客户设备无法接受视频。将客户的设备重新启动上电,测试913的电压1.8V正常,913分频有12M时钟输出,摄像头工作正常,客户设备正常接收视频

请问哪边有问题?913和914是否有工作前后次序?

2.    913 LVDS数据输出需要串联50V 0.1uf 电容,我司采用25V 0201 0.1uf电容是否有问题,请问为什么需要耐压这么高?

3.  外部晶振模式和PCLK模式,请问哪个模式更稳定,因为有些样品出现图像闪屏