This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH2180在输入端和信号源之间串一个500欧左右的电阻,在60Mhz@100mv输入信号下,输出强度基本达到100mV,为什么??

LMH2180YD/NOPB这颗料我们在使用中问题如下:

 LMH2180YD/NOPB 这颗料-3dB带宽到不了手册上描述的68MHz,具体原理图和测试波形如附件,这个问题比较急,请正面回答,尽快回答,谢谢。

测试温度:常温25度

测试环境:室内-联调房

信号发生器:agilent E4432B

具体测试步骤:

1、芯片3.3V供电,断开原理图中C134,在输入100mVpp  62Mhz信号时,out1与out2输出仅为33mV,与手册描述差异比较大,如手册中figure 3中曲线左移,即-3dB带宽性能变差,只有在输入30Mhz以下信号时,输入与输出才能保持1比1输出。

2、芯片改成5V供电,带宽性能依然无改观。

3、电源增加10uF电容,EN端增加100nf电容与510K电阻,在第一级输出端增加30Kohm负载,并断开第二级 LMH2180YD芯片电源,带宽性能依然无改观。

4、在无任何元件的PCB板上对此物料进行带宽性能验证,依然无改观。

图1,原理图

图2,输入波形,耦合电容前后基本无差别。

图3,输出波形,加30Kohm负载;接后级buffer,悬空 三者基本无差别。