This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近使用SN65HVD230 3.3V 做了几件产品,但在接入CAN网络时发现只能接收数据不能发送数据。
CAN网络其他器件使用的CTM1050 (5V)
电路图为:
调试过程为:
1.Vref接3.3V,单独通信正常,放入CAN网络中只能接收不能发送
2.Vref接3.3V/2,无反应
3.Vref接地,单独测试能接收,一发送就出错
4.Vref接CANH--60Ω--60Ω--CANL的两个电阻之间,现象同上
问题:
1.该如何解决这个问题。
2.CTM1050的CAN线上有CANG,应如何处理。