TI工程师好:
最近我在使用DS90UB913A/ DS90UB914A串并转换芯片,电路做好后,我在914这一边控制GPIO高低变化,913那边可以同步变化,说明硬件OK,但是发现913输出低电平VOL是0.8V,有些偏高,请问这是什么情况? 我VDDIO是1.8V, 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI工程师好:
最近我在使用DS90UB913A/ DS90UB914A串并转换芯片,电路做好后,我在914这一边控制GPIO高低变化,913那边可以同步变化,说明硬件OK,但是发现913输出低电平VOL是0.8V,有些偏高,请问这是什么情况? 我VDDIO是1.8V, 谢谢!
你的意思是913的GPIO输出高电平Vol=0.8V?那么SDA和SCL低电平是否正常?SDA 和SCL也是VDDIO供电,上拉电阻多少?
I2C上拉到VDDIO,4.7K,913的SDA为高18V, SCL为0.45V,最高有0.5V的,每个芯片都还不一样,,914这侧还没有灌入I2C信号恒定上拉到VDDIO,现在需要GPIO控制,暂时跟I2C功能无关,谢谢