This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ISO1050DUBR/TI/R-PDSO-G8
我们在测试控制器耐低温过程中,发现了问题,请你们技术帮我们分析下。具体问题如下:
智能化测试控制器耐低温,控制器放在冷库中-20℃持续1小时控制器CAN信号中断.对ECU产生干扰,拔掉CAN线ECU恢复正常.控制器参数、监控界面正常.
测试耐低温控制器只接了电门锁,电机温度与仪表CAN通讯线路. 拿出来等温度上升CAN信号正常.
ISO1050可以工作在额定工作环境温度范围为-55C~105C,是否是MCU还是其他元器件的工作环境温度没有满足您的需求,建议CANH和CANL总线上加屏蔽线。