Other Parts Discussed in Thread: LMH0344, LMH0341
现在载荷单位用Gennum公司的GV2970,将16位的并行数据转换成SDI信号数据,其中每个分量的最低2位接的都是低电平,也就是说发送的SAV和EAV为:FF3FCH、00000H、00000H……; 我用贵公司的LMH0344和LM0341+xilinx Kintex 7做SDI的接收,用贵公司提供的模块解析信号。我接收市场上的商用1080p摄像头时都没有问题,都能采集到正确的图像数据。
我有三个问题:
1)载荷发送的这样的SAV和EAV用对LMH0341的解扰是否有影响?
2)现在用sony的 LMD-091W监视器接收载荷输出的信号,并识别出信号为1080p25。而我的FPGA则识别不出正确的信号,用在线示波器采集解扰后的20bit数据,发现Y分量和UV分量的SAV和EVA有时前后错位了一个时钟周期;有时UV分量SAV/EAV有效时,Y分量则没有对应的SAV/EAV;有时UV分量SAV/EAV有效时,比如UV的分量为FFH,00H,00H,9DH,而Y分量为3FH,00H,00H,1DH;针对以上这样的情况,烦请分析一下我们接收与sony监视器区别?是什么原因导致解扰后的20bits数据不正确?
3)我推测应该是LM0341解析出的5对LVDS数据和1对LVDS时钟,进入FPGA后,FPGA模块中DDR数据采集有问题,针对该问题我想通过在FPGA内部调整LVDS数据对LVDS时钟的延时实现正确采集,我如何确定每一路应该延时多少呢?还有我还想通过训练每个bit,做一个相位自适应调整的模块,请问每一路LVDS数据在连接建立时有没有特殊的训练序列,如果有训练序列是什么?
谢谢了!