This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于8位eMMC数据线2:1开关选选型问题

Other Parts Discussed in Thread: TS3A27518E, TS3DDR3812, TS3DDR4000, TS3DV642

最近有一项目,需要在智能手机方案之上另外增加一个eMMC芯片,

大概要实现的功能是实现双系统,即两个eMMC芯片中分别放不同的系统镜像文件,

在开机时通过组合建的方式来选择处理器加载哪一块eMMC,引导哪个系统。

因此,需要选一片能够切换两个8位eMMC芯片数据线的芯片。

了解到TS3A27518E可以实现此功能,但其只有4位数据线,与8位相比还差4位。

想到同时用两片TS3A27518E并起来用,但又担心功耗会上去,且PCB面积紧张、有限。

最近一直在寻找合适的方案,另外还了解了TS3DDR4000、TS3DDR3812、TS3DV642这3款芯片。

TS3DDR4000是用于切换DDR数据线的,不确定能否用在MMC数据线上,还有就是备货是个问题。

TS3DDR3812也是用于切换DDR数据线的,备货还好,但似乎也不兼容1.8V的IO电压。

TS3DV642是用于切换HDMI之类的差分信号线,也不确定能否用在MMC数据线上。

大家有做过类似功能方案的可否推荐几款芯片做参考。感激不尽!

大概的要求如下:

1.能实现12位,2:1开关功能;

2.IO能够兼容1.8-3.0V电压;

3.主供电能够满足1.8-3.3V;

4.小封装尺寸,最好是BGA封装;