Other Parts Discussed in Thread: SN74AVC16T245
请教一个关于sn74Avc16T245的问题,
我的电路在3.3V->1.8V工作完全正常,输出波形电压清晰,边沿稳定无噪声。
但是在1.8V->3.3V时,输出波形的边沿出现了明显的毛刺,幅值很明显,每个周期都波形都有这个毛刺,有时甚至会干扰到FPGA对时钟沿的判定。
请问:在升压电平变换(1.8->3.3)的过程中产生这个毛刺的现象是正常的么?有没有什么方法避免这个干扰呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. A路给的是3.3V还是1.8V?两个DIR和~OE给的是几伏的逻辑?
2. 你3.3V那一端的输出负载有多大?输出电流有多大?最好能上个电路图。
3. 换个片子上去,看看还有没有类似问题。
Decapton Wang 说:1. A路给的是3.3V还是1.8V?两个DIR和~OE给的是几伏的逻辑?
2. 你3.3V那一端的输出负载有多大?输出电流有多大?最好能上个电路图。
3. 换个片子上去,看看还有没有类似问题。
您好,
1、A路给的1.8V,两个DIR和OE都给的是VCCA的逻辑,即1.8V。
2、3.3V那一段接的是ALTERA fpga的IO口,负载很小,电路不会超过ma,也就在100UA以内吧~
3、好几个板子都是相同的现象,估计能够初步排除芯片的额故障问题。除非是这一批次的芯片出现问题,但可能性应该很小。
附上了相关的电路图
非常感谢~
手册上只是指出四个控制脚是由VCCA供电,但是并没有说要DIR接一个10KΩ的上拉电阻,也没有说~OE要接一个1KΩ的下拉到地,建议把这四个电阻换成0Ω试试。还有就是检查一下1.8V和3.3V共地和不共地时,效果会怎样。
直接0Ω,先试试看结果怎么样。如果还是有问题,试试看把供电用比较干净的稳压电源效果怎么样。
那用3.3V的电压驱动四个控制脚,看看输出特性是怎样的。从电路图上看不出什么问题了。
难道在3.3V那一侧有端接的要求?可是那边只是一个FPGA的IO啊。要不在3.3V那端的串联一个50Ω以内的小电阻试试看。