Other Parts Discussed in Thread: CDCE62005
大家好,在CDCE62005的Aux input管脚加了一个25MHz的晶振,但是上电之后cdce62005没有频率输出,看数据手册应该有默认的输出的,我们首先将SPI_CS一直设定为3.3V,将cdce62005的power_down管脚置为0,然后将power_down置为高电平,可是频率没有输出,请问我们如果就想输出cdce62005中EEPROM默认的频率的话,需要配置62005的寄存器吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CDCE62005
大家好,在CDCE62005的Aux input管脚加了一个25MHz的晶振,但是上电之后cdce62005没有频率输出,看数据手册应该有默认的输出的,我们首先将SPI_CS一直设定为3.3V,将cdce62005的power_down管脚置为0,然后将power_down置为高电平,可是频率没有输出,请问我们如果就想输出cdce62005中EEPROM默认的频率的话,需要配置62005的寄存器吗?
62005里面有个smartmux,可以切PRI_in,SEC_in和AUX_in,你看看你的电路里有没有配置这个smartmux。输出的分频器同样有切换功能,可以切到smartmux,VCO,你看看输出有没有配对。
Decapton 你好
感谢你的回答,我查看了默认的寄存器配置,发现是由Aux_in这一项的,默认的配置是优先选择PRI,其次是SEC,最后是Aux_in,在我们的板子上,pri和sec都是浮空的管脚,那么CDCE62005是不是会默认选择AUX_IN呢?
应该不会,还是需要你配置。从EVM板的GUI软件上来看,smartmux里有5种选择,分别是PRI,SEC,AUX,AUTO first PRI then SEC,AUTO first PRI then SEC then AUX。对应RAM寄存器是Register 5。所以这样看来,如果不对这一项在Register 5里做配置,应该不会默认选择AUX的。