This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE62005寄存器配置

Other Parts Discussed in Thread: CDCE62005, CDCE62005EVM

大家好,在CDCE62005中的EEPROM里面有8个寄存器,RAM中有9个寄存器,请问当上电之后,第九个寄存器的值怎么确定的呢?每次上电都需要通过SPI端口往第九个寄存器里面写值吗?

  • 这样理解不对吧,从手册第7页的文字来看,上电时,RAM可以从EEPROM里复制配置信息,从而在没有主机与62005通信时配置这颗芯片。也就是说,如果EEPROM里已经写好配置信息,那么上电后可以不做额外的配置,直接用EEPROM里的默认配置。另外,虽然RAM里有9个寄存器,但是里面很多是工厂专用位和保留位,所以RAM里的9个寄存器和EEPROM里的8个寄存器,应该不是一一对应的。

  • 通过SPI配置CDCE62005寄存器,实际上是配置RAM上的9个寄存器的,一般在EEPROM unlock的情况下,RAM才能将配置写入EEPROM,至于你所说的RAM与EEPROM的对应关系这个就不确定了,肯定不是一一对应的。

    至于寄存器的配置,要么就是查表来完成配置,要么使用CDCE62005EVM GUI可以直接生成你需要的寄存器配置。