This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教-DS90UB913和914做同轴电缆视频传输时易受手机干扰

大家好,我们正在用TI的DS90UB913和914做同轴电缆视频传输,目前发现有个问题,就是当通话中的手机靠近同轴电缆的时候,视频会出现丢帧现象,画面出现大面积紫色区域,当手机拿走后又自动恢复了。经测试干扰的时候Locked信号会变成低电平(正常时候Locked应为高电平)。我仔细看了一下913和914的手册,发现推荐模式是使用外部晶振(我们目前使用的是Imager Sensor的pclk作为913的时钟),所以我想改成使用外部晶振给913提供时钟,但麻烦就来了,如下:
我们现在使用的是sony的IMX222传感器,此传感器只支持37.125MHz的时钟输入(还支持54MHz的时钟,但视频输出格式不能满足要求),PCLK输出是74.25MHz(12bit模式),因此我们只能设置913工作在12bit高速模式。此时要求PCLK和外部晶振的倍数是1.5,也就是49.5MHz,也就是说只能选择49.5MHz的晶振给913提供时钟,然后913二分频出来的24.75MHz是要给Imager sensor做参考时钟的,因此我必须将24.75MHz倍频1.5倍到37.125MHz给sensor做参考时钟。我想问一下,这样倍频有没问题(因913给的参考是没有倍频的,913举的例也不合适我们使用)?还有如果可以这样使用,有没推荐的电路或倍频电路?如果不能这样使用,有没有解决方案?或者手机干扰有没其他的解决方案?
谢谢!