This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB964 问题咨询

MIPI CSI2的clock这边,按照规范有2种工作模式,一种是clock 连续的模式,一种是clock不连续的模式(这种中间会出现0x6f0),我们要求用连续的模式。(这个是imax6要求)

看964 规格书 ,寄存器0x33 确实有位1 设置clock 模式的 

 CSI_CONTS_CLOCK RW 0 Enable CSI continuous clock mode

0: Disabled

1: Enabled 

我们现在开启这个这个持续模式, 发现出现错误 receiving a DDR clock

帮忙看下这个CSI_CONTS_CLOCK 是不是需要跟其他寄存器一起配合配置呢?

     请帮忙确定下之前DS90UB964+i.mx6Q时,964是什么样的配置? 例如400Mbps/800Mbps, Raw10等, 多谢支持!