Other Parts Discussed in Thread: TXB0302, SN74AVC4T234, TXB0304, SN74AVC2T244, LSF0108, SN74AVC16T245
需要对一批流片的芯片做测量,芯片供电电压1.0V,需要对外来的SPI信号做电压转换,不知道使用哪一款芯片好,请求推荐!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TXB0302, SN74AVC4T234, TXB0304, SN74AVC2T244, LSF0108, SN74AVC16T245
需要对一批流片的芯片做测量,芯片供电电压1.0V,需要对外来的SPI信号做电压转换,不知道使用哪一款芯片好,请求推荐!
参考TXB0302可以实现1V到3.3V电平转换。您的SPI频率多少?需要注意TXB0302能够支持的最大 data rate。
使用MSP430(8M晶振)产生的软件模拟SPI,频率应该不高。
看了一下TXB0302或是TXB0304为2或4位,有相似功能的SN74AVC2T244、SN74AVC4T234是2位的。请问TI有符合要求的,位数更多的芯片吗?
SPI就是4bit的,您需要几位的?看下LSF0108,8bit,但是一般实现的是0.95V到其他电平转换。
其实8bit,16bit的电平转换很多,能够应用在SPI上的也不少,但一般最低电压在1.2V左右。
嗯。SPI是4bit,不过我们设计成多路SPI的形式。原来使用的是16bit的SN74AVC16T245,现在因为工艺换了,所以要找1.0V 16bit的。不过看来是没有了