This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925与DS90UB928的I2C数据透传问题。

条件:

    1.想利用DS90UB925与DS90UB928实现I2C数据透传,不知如何设置DS90UB925寄存器;屏幕端的DS90UB928属于已正常功能使用的汽车中控屏幕端,想自己设计MCU软件与DS90UB925适配替换汽车汽车中控主机,并实现与汽车中控屏幕(DS90UB928)的触摸数据读取。

    2.现在MCU与DS90UB925的I2C通信OK。

问:

    1.如何设置DS90UB925寄存器实现I2C数据透传;

    2.现在通过DS90UB928的I2C口没有抓取到相应数据.

  • 先确认下你的应用:MCU-----DS90UB925-------DS90UB928------remote slave是吗?

    现在MCU和925的通信已调通,需要MCU和928以及remote slave的通信是吗?

  • 是的,通过DS90UB925与DS90UB928的通信,实现连接到DS90UB925稍微MCU与连接到DS90UB928端的MCU进行数据交换。

  • 恩,关于这种I2C通信具体寄存器的配置方法,建议参考这篇应手册snla222.pdf。它是以DS90UB913&914为例,详细介绍进行寄存器的配置。

    如果对其中的讲解有任何问题,大家可以一起讨论。

  • 目前我们使用UB927与屏幕端的928尝试连接,但是在I2C通讯上,还不能建立与928的联系,请问,可以参考哪里?谢谢。