1. 我们需要用DS90UB925/926的I2C控制Panel的Touch IC,请教几个问题:
1, DS90UB925/6的地址是否只能通过IDX PIN来设置?能否用软件设置?
2, TOUCH IC除了I2C控制还有终端信号INT,能否用DS90UB925/6的INTB PIN来传输终端信号?
3, 如何配置DS90UB925/926和TOUCH IC主从关系,实现主机远程控制?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是的,通过接在IDx上分压电阻的值大小来确定从机地址,最多可挂接9个不同的地址,详细可参考Table5.
DS90UB925和926的INTB PIN直接相连,你指的是通过控制INTB PIN来控制TOUCH IC的中断信号?
确认下你的应用,主控是和925接还是926接? HOST----DS90UB925----926-----Touch IC,是这个应用吗?