Other Parts Discussed in Thread: TS3DV20812, TS3DV642, DS90CR288A, DS90CR287
应用中有两路CameraLink输入,可以用TS3DV20812或ts3dv642这类的复用器进行切换吗?
另外,CameraLink发送端为芯片DS90CR287,若经过切换芯片后,再用DS90CR288A接收,对信号质量是否有影响?
请推荐合适的设计或芯片,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TS3DV20812, TS3DV642, DS90CR288A, DS90CR287
应用中有两路CameraLink输入,可以用TS3DV20812或ts3dv642这类的复用器进行切换吗?
另外,CameraLink发送端为芯片DS90CR287,若经过切换芯片后,再用DS90CR288A接收,对信号质量是否有影响?
请推荐合适的设计或芯片,谢谢!
一路Camera link是1对clock pair,4 对LVDS data? TS3DV20812是可以进行LVDS信号的切换,另外还要看下能支持的data rate是否够用。
经过开关器件之后,由于开关的Ron很小,输入输出除了有一定的延迟之外,幅值基本上不会改变,后端再接接收器件是没问题的。不知您是否考虑的这个方面
DS90CD287的data rate最大为2.38Gpbs。在选取switch时,switch支持的最大带宽我们一般推荐3倍的余量,也就是说,2.38Gbps/2=1.19GHz*3=3.57GHz,switch的带宽至少3.57GHz最好。 从这点来看TS3DV642符合要求,它的带宽能支持到7.5GHz。
如果您的应用是1pair clock+4对data的话,那么实现2:1的应用,每个信号源要5路信号,switch需要10路差分信号进行2:1切换,TS3DV642又不满足需求。
因此看了下TI的高速信号开关,好像没有符合需求的。