1、采用PIN config模式时,两片ds80pci800/ds80pci810芯片怎样配置成X16?
2、原理中未添加EEPROM电路,是否对X16配置会有影响,也就是说要配置成X16是否一定需要通过EEPROM配置才行?
3、附件是我做的原理,请帮忙审核是否会有问题?
4、若无问题,我要如何配置,才能调出X16的带宽?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、采用PIN config模式时,两片ds80pci800/ds80pci810芯片怎样配置成X16?
2、原理中未添加EEPROM电路,是否对X16配置会有影响,也就是说要配置成X16是否一定需要通过EEPROM配置才行?
3、附件是我做的原理,请帮忙审核是否会有问题?
4、若无问题,我要如何配置,才能调出X16的带宽?
从ds80pci800的内部架构来看,是4lane的,所以如果需要配置成PCIE x16的话,需要4个ds80pci800才行。
不论是使用单个ds80pci800,还是采用多级相连,都是三种配置模式,Pins/SMBus/Direct-EEPROM,也就是说不一定使用EEPROM配置。
如果多个ds80pci800相连,采用EEPROM模式的话,建议参考http://www.ti.com/lit/an/snla228/snla228.pdf。
PIN config 模式就是通过控制引脚来进行equalization/ de-emphasis,RATE等的设置,而EEPROM模式则是通过软件进行这些参数的配置。
如何调试的话,我想应该是有专门调试X8或者X16的测试治具,也是看眼图的波形。
参考电路的话,采用4颗DS80pci810配置成X16,可以参考https://www.ti.com/seclit/df/tidrd10/tidrd10.pdf
目前我司测试的情况是这样的:
1、PCIE-X16插槽采用标准PCIE-X16的显卡进行测试,主板CPU到PCIE插槽之间采用了4片DS80PCI800芯片,系统下采用GPU-Z显卡测试软件测试显卡实际工作带宽,软件测试结果显示的是X16的显卡实际工作在X8的模式下,显卡本身不存在问题,也就是说在我们的设计中,只有PCIE-X16的前8个lane起作用了,后8个lane没有调通,所以不知道我们的设计中是否哪出了问题,想问一下贵司怎样才能使X16的后8个lane起作用,我们的原理图也上传了,不知是否存在问题?
2、我看DS80PCI810的参考原理的上下拉电阻有249和4.99K,我们用的是1K和20K,不知处阻值大小是否会有影响?
3、还有DS80PCI800的PRSNT信号,我们电路中4个芯片的此引脚全是下拉,不知此处是否也有影响?