Other Parts Discussed in Thread: SN65HVD1040
can收发芯片SN65HVD1040如何与tps65381的canwu连接起到唤醒作用? 我的理解是在休眠模式当收到can报文时,rxd发送一个低脉冲。请问该如何连接呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN65HVD1040
can收发芯片SN65HVD1040如何与tps65381的canwu连接起到唤醒作用? 我的理解是在休眠模式当收到can报文时,rxd发送一个低脉冲。请问该如何连接呢
从tps65381的datasheet来看,CANWU是连接在外部的CAN 收发器上,我们是想CAN收发器上有这么一个wake up引脚可直接连接,但是看了下目前带有wake up功能的CAN收发器都没有这个引脚。我想单独对于tps65381的wake up来说,可以通过主控来控制这个CANWU电平进行唤醒。或者按照datasheet上的直接将 IGN 和 VBATP通过一10Kohm接在一起 If the application does not require wake up from IGN (ignition or KL15) or wake up from CANWU (a CAN or other transceiver), but the device should wake up any time power is supplied, one method is to connect IGN to VBATP (and VBAT_SAFING) through a 10 kΩ or greather series resistor。
对于SN65HVD1040来说,您的理解是对的,休眠模式,RXD应该一直是处于高电平状态直到收到一个有效的WUP(wake up pattern)时会拉低。
SN65HVD1040对于wake up介绍的不是很详细,可以参考TCAN1042的datasheet,里面介绍的非常详细。