用TFP410用作灰度图像传输,前端CPU输出VS,HS,DE,PCLK,8位图像数据,芯片工作在24位模式,将红绿蓝三路端接在一起,后端用TFP401A进行解码,两者只连接了TXC+,TXC-,TX0+,TX0-,后端TFP401A解码后只有VS和HS信号输出,DE基本都是噪声,来来回回把电路图审查了好多遍,认为电路图正确,就是DE不能正常输出,不知道会不会是因为没有连接TX1+,TX1-,TX2+,TX2-的原因?不知道论坛有没有人这样用过?手册也没有明确说这样用不行!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
非常感谢您的反馈,如果您当时只接了一组data,可以看下输出SCDT的状态应该输出的是无效的link,因为单link的DVI包含了一对clock,三对data。这是一个完整的T.M.D.S link.