This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于使用LMX2592锁相环输出带调制信号的问题

Other Parts Discussed in Thread: LMX2592, PLLATINUMSIM-SW

     想用LMX2592实现带调制的频率源,输出中心频率为6.8GHz,调制深度1.2kHz,调制频率120Hz的信号。在实验过程中发现,输出单频点的6.8GHz信号没有问题,但通过程序修改输出频率时,每修改一次频率值,在频谱仪上会看到杂频闪现。如果以120Hz的速度修改输出频率(在6.8G左右600hz跳频),相对于6.8G单频时出现大量杂散频率。请问,修改小数N分频器瞬间产生噪声是锁相环固有特性吗?有没有办法可以消除或减小?

    修改输出频率时,只修改R44和R0寄存器,其中reg44_data变化量大约8bit。

    WriteOneByte(reg44_data);//R44

    WriteOneByte(0x00227C);//R0

   

  • 推荐使用最新的PLLatinum Simulator Tool进行PLL相位噪音仿真,包括其他一些噪音源,比如输入噪音,filter,输出divider带来的噪音都可以进行仿真。

    http://www.ti.com/tool/PLLATINUMSIM-SW?keyMatch=PLLatinum%20Sim&tisearch=Search-EN-Everything#1