This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2531输入晶振频率确认

Other Parts Discussed in Thread: LMX2531, LMX2541

我现在碰到个问题,利用LMX2531产生一个960MHz的时钟,但是OSCin的频率我却使用了100MHz,而发现文档中要求最大为80MHz,现在想请教下如果我把这个100MHz的晶振输出通过芯片进行二分频或者四分频,但是分频出来的信号时方波,这样子可以么?谢谢大家

  • 从手册第9页看,你需要用其他的芯片做分频,2531内部的R divider最高只能接受80MHz的输入时钟。分出来的基准时方波问题不大,因为即使一个正弦波进2531,内部的buffer也会把它整形成方波的。需要注意的是

    1. 手册第6页电路图中标明的100nF交流耦合。

    2. 手册第9页指出VOSCin的范围是0.5~2Vpp。

  • 参考可以是方波, lmx2531参考小于80M,你也可以用lmx2541

x 出现错误。请重试或与管理员联系。