This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TUSB8041中Port Used Configuration Register的设置



在数据手册中,该寄存器类型为RW,且称“All combinations are supported with the exception of both ports 1 and 3 marked as disabled.”这是否意味着可以写入该register从而将port至为disable?如果可以,请问HUB内部的逻辑是将PHY至为disable,还是将PWRCTL至为disable,或是其他逻辑?

谢谢!

  • 这个寄存器的作用四个下行端口的使能配置,bit0代表的下行端口1,bit1代表的端口2,以此类推。

    All combinations are supported with the exception of both ports 1 and 3 marked as disabled这句的意思是说排列组合方式都能支持,除了将port1和port3 disable之外。

    disable的意思比如bit0=0,说明下行端口1 disable掉,而不是PWRCTL disable。