This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913工作不正常



Ti 工程师

       你们好,我在调试913的过程中,遇到了几个问题,可以帮我分析下吗

        开发环境: ADAS + 964 + 913 + sensor(ov5640),

      913采用用PCLK模式(sensor 自己提供24MHZ clk), 当ADAS通过964/913配置好sensor后,给sensor power on(write 0x2 to reg 0x3008),后, 913 和 0v5640的 i2c通信就不稳定了,ADAS读写913或者5640的寄存器经常出错,开始怀疑5640输出的PCLK不符合913的要求,可是读913的0xC寄存器值为0x15,bit2

为1表示valid PCLK detected,PCLK输出为84MHZ,请问下这是什么原因造成的,谢谢

      当913采用外部晶振,GPIO2 24MHZ给sensor提供clock时,不管怎么配sensor,都不会出现i2c不稳定的情况,可是PCLK非常不标准,测得的频率为23.8M

HZ,为什么同样的配置都是24MHZ输入,得到的PCLK会不一样