This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913和DS90UB914传输图像数据的问题



1,硬件结构组成:前端采集部分用MT9V032+DS90UB913组成;后端接收部分用DS90UB914+FPGA组成,做FPD-LINK的传输测试实验

2,913和914的寄存器没有做配置;MT9V032的sensor直接用FPGA做I2C配置的;现在的现象是用altera fpga的signal tap抓波形观察,发现帧同步、行同步、像素时钟、LOCK信号均正确,只是有效的8位像素数据没有变化,是一个定值0x20,请问导致这种现象的原因有可能是哪些?

3,由于MT9V032的I2C寄存器读写操作都是16位的,通过914的alias映射怎么进行16位的I2C读写操作?

4,913和914的寄存器一般需要配置哪几个?