Other Parts Discussed in Thread: ALP
大家好,
调试964发现无图像输出,开发环境为 ADAS+964+913++sensor,964 和 913 使用同轴电缆连接,目前只接了一个913
913采用PCLK模式,
配置好sensor后PCLK HSYNC VSYNC信号都正常,PCLK输出48MHZ,sensor 配置为1280x720 30fps raw 8bit data输出
但是964无信号输出,读964的状态寄存器:
964 reg 0x35 = 0x1 说明 TX port pass
964 reg 0x73= 0x2 line count H
964 reg 0x74= 0x37 line count L (0x73,0x74的值一直在变化)
964 reg 0x75 = 0x2 line length H
964 reg 0x76 = 0xfd line length L (0x75, 0x76的值固定不变)
964 reg 4d = 0x3
964 reg 4e= 0x45
964 reg 4f = 0x18 (24MHZ ?)
964 reg 50= 0x0
964 reg 55 = 0x0
964 reg 56= 0x0
说明964接到数据了,可是964没有信号输出,小弟实在毫无头绪,请求各位大神给点建议,谢谢!
964
913