This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83640与DM4818 RMII通讯问题求助!!

Other Parts Discussed in Thread: DP83640, ETHERNET-SW

用到DP83640与 DM4818   RMII通讯,dp83640连接到dm8148的EMAC1,测试发现网络无法正常工作

现象描述:接上网线时RJ45的link亮,Linux可以读取到DP83640的id;用PC ping 开发板时RD0、RD1用示波器可以看到波形;ping 网关时TD0、TD1用示波器看到波形,RJ45的黄灯会闪烁,但是没有返回数据(ping失败);查看驱动的统计信息,发现接收数据为0;

配置: DP83640 使用RMII主模式

1)      Pinmux of EMAC1

RMII_REFCLK  0x48140B9C:  00040001

GMII0_TXD2    0x48140BEC:  00000002

GMII0_TXD3   0x48140BF0:  00000002

GMII0_TXD4   0x48140BF4:  00000002

GMII0_TXD5    0x48140BF8:  00000002

GMII0_TXD6    0x48140BFC:  00000002

GMII0_TXD7    0x48140C00:  00000002

GMII0_TXEN    0x48140C04:  00000002

GMII_SEL Register  0x48140650:  00000106

RMII_REFCLK_SRC  0x481C52E8:  00000001