This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
主控可以输出的MIPI DSI 信号,同时还有另外一个通道只能输出是LVDS 信号,那么就需要通过一个switcher 转换为 MIPI 4LANE DSI 输出到一个LCD 上,TI 是否有这种芯片的?
如果您的意思是输入有LVDS,有MIPI信号,想通过switch输出MIPI,这样的话可以考虑TS3DV642这款,这款是一个多通道的2:1/1:2开关器件。
换句话说,正如您前面的帖子,这款switch不能实现输入LVDS,输出MIPI, 比如D0接MIPI,D1接LVDS,通过使能端控制D0和D0A导通,其他输出均HI-Z。
当然如果您的LVDS可以是4 pair。