This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于SN65LBC175的应用

Other Parts Discussed in Thread: SN65LBC175A, SN65LBC174

各位专家:

   我现在应用SN65LBC175A这款芯片时,经常会烧坏,没有查出原因,我想咨询一下,一般什么情况下,这款芯片比较容易烧坏,它另外的接口能和SN65LBC176D进行搭配使用吗?

  • 1. 你的电源如果是从直流稳压电源给的,可以监测一下工作时的电流是否在手册允许的范围内。同时,检查输入的共模是否在-7~12V以内,输入的电流是否过大。注意手册有说明,输入共模12V时,最大输入电流0.9mA;输入共模-7V时,最大输入电流-0.7mA。检查输出电流,手册建议值是+/-8mA,看看你的应用是不是超过了。

    2. 从手册上应该能和176搭配。不过176是可收可发,如果和175用,那就只能用作发送了,有点亏。不如照175手册所述,和SN65LBC174搭配,这样比较物尽其用。

x 出现错误。请重试或与管理员联系。