This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9555 pin脚配置没反应,全部为1

Other Parts Discussed in Thread: TCA9555

主为xilinx的zynq-7000的I2C,挂了两个TCA9555 一个从地址0x20,另一个从地址0x21,频率100k,

补充硬件:VCC 3.3V,SCL,SDA,INT上拉电阻为4.7K,A0直接接3.3V,A1,A2接地。

这里只给0x21写数据

先初始化:

write (Config_Reg0)0x06  0x00

write (Output_Reg0)0x02  0xFF

write (Polarity_reg0)0x04  0x00

write (Output_Reg0)0x02  0xAA

但是引脚电压依旧为高,没有改变

时序图如图

第一个是SCL,第二个SDA,第三个INT

频率改到400k接收不到ACK信号

  • 主为xilinx的zynq-7000的I2C,挂了两个TCA9555 一个从地址0x20,另一个从地址0x21,频率100k,

    补充硬件:VCC 3.3V,SCL,SDA,INT上拉电阻为4.7K,A0直接接3.3V,A1,A2接地。

    这里只给0x21写数据

    先初始化:

    write (Config_Reg0)0x06  0x00

    write (Output_Reg0)0x02  0xFF

    write (Polarity_reg0)0x04  0x00

    write (Output_Reg0)0x02  0xAA

    但是引脚电压依旧为高,没有改变

    时序图如图

    第一个是SCL,第二个SDA,第三个INT

    频率改到400k接收不到ACK信号

    请TI专家回答一下,坐等。。。。。。

  • 将从机地址0X21<<1为0X42试试,从机地址不正确也是导致不产生ACK的原因。

  • 0x42试了一下,接收不到信号了。显然不是从机地址的问题。您再分析一下了