This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你是想用这颗芯片做buffer还是时钟产生?如果只是做buffer,不走内部的PLL,那可以用,输出的LVCMOS口最高可以支持到160MHz。如果是用作时钟产生,注意一下内部的PLL调谐范围是80MHz~230MHz。对于64.8MHz,你需要让PLL振在129.6MHz或194.4MHz;对于95.3MHz,你需要让PLL振在95.3MHz或190.6MHz。因为64.8MHz和95.3MHz是“互质”的,最小公倍数是6175.44MHz,所以CDCE913的PLL没办法振出来这样一个频率,使得一片CDCE通过对PLL的分频,同时得到64.8M和95.3M。如果用切换的方法,你需要选一块合适的晶振,使得这块晶振和CDCE搭配时能得到64.8M或者95.3M的输出时钟。
我是想用这颗芯片代替原来的有源晶振,该芯片的输出口为LVCOM,是不是输出的波形是方波?我想要输出正弦波用于混频,不知道这个芯片可不可以?不可以的话可不可以帮我推荐一款别的芯片?
如果一定要输出正弦波,那么这颗芯片不行,因为从手册第1页的框图来看,这颗芯片的输出都是LVCOMS的,是方波。如果一定要正弦波输出,可以考虑LMX2541,不过,需要提醒的是,64.8M/95.3M这两个频率太怪,最小公倍数是6175.44MHz,没有办法用一个LMX2541的PLL振出这样一个频率。