This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ti 工程师,
您好!
我的开发环境是这样的 sensor + 913 + 964 + MCU.
使用官方购买的913开发板 是可以正常工作的
但使用ti-00421方案,做的913的模块,i2c通信不正常,读964的寄存器0x5b值为0xb0,说明913的i2c地址被正确加载,
但是却访问不到913的寄存器。不知道什么原因。
比较了下913 EVM和ti00421方案的原理图,发现913的vddio 为3.3V,但是ti-00421方案为1.8V,不知道是不是导致工作不正常
你得确认下913这边电压是否正常。也可以把913的I2C飞到MCU端测试下。
谢谢你的回复,电压都正常,使用ti-00421的方案作了四个camera,只有一个913模块可以读到寄存器,看913数据手册,pdb上电有时序要求,要接个10uf的电容,
但是ti-00421原理图没有接,不知道这个有没有影响
手动控制一下PDB的时序试试呢?当VDD_n和VDDIO都上电起来到稳定之后,PDB再由低变高。验证下是否PDB导致的。