手册上写portA 输入-0.5~4.6,portB 输入-0.5~6.5;
如果我Vcca接3.3V,Vccb接5v,然后portA输入 5v的信号,那么输出端portB输出的是什么??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
手册上写portA 输入-0.5~4.6,portB 输入-0.5~6.5;
如果我Vcca接3.3V,Vccb接5v,然后portA输入 5v的信号,那么输出端portB输出的是什么??
PortA的 VCCA=3.3V的话,那么A input不允许超过VCCA=3.3V。 所以5V接Aport是不允许的。
是的,超过它的工作电压范围,很有可能烧坏。jignxiao han 说:如果接了5V的话,会把芯片烧掉吗?
您是需要74hc245这类缓冲器,或者其他什么要求,需要电平转换吗?
参考下SN74LVC2T45这款。jignxiao han 说:但是体积不能大,最好是2路的器件,只是加在串口上
这个我也有看过,和txs0102有什么区别吗。看datasheet差不多
区别主要有两点:1)TXS是不带方向控制为的,SN74 是通过方向控制端来控制A到B还是B到A。jignxiao han 说:这个我也有看过,和txs0102有什么区别吗。看datasheet差不多
2) TXS或者TXB的驱动能力很弱,datasheet中也有介绍,如果需要驱动负载,建议使用SN74系列。
我需要2路的电平转换芯片,一端是coms电平,一端是ttl电平,要双向转换,3.3-5v,请问有什么芯片可以选择,最好是自动双向的,不用控制方向的?