This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CMOS输入电压问题

CD4081与门仿真时的输入电压一个是VCC另一个是0.3VCC-0.7VCC.输出电压为0.5VCC,是为什么

  • VCC是多少V?试试把0.3VCC~0.7VCC增大,变成0.2~0.8,或0.1~0.9,看看有没有改善。可能是输入幅度不够,芯片直接把输入当成“X”(未知)了。

  • 仿真时VCC是5V,因为cd4081是cmos,输入电压小于0.3VCC时看做低电平  大于0.7VCC时是高电平  我不知道中间区域应该是什么样的  属于放大区吗

  • 5V供电时,VILMAX不能大过1.5V,VIHMIN不能小于3.5V。你用错了。你用的那个区域,正好是芯片不能分辨高和低的区域。这个中间区域对CMOS来说,应该叫饱和区,对应bipolar的放大区,但是在逻辑应用里,应该避免芯片工作在这个区域。