咨询一下:若使用Altera cyclone IV 和 cyclone V系列的FPGA,连接 LVDS buffer ,传输速度达到600Mbps,传输距离是否可以达到10m及以上?
另外,FPGA的管脚电压为2.5V,选择哪款 LVDS Buffer合适呢? 目前看到一个DS90LV804的芯片,电源电压为3.3V的,不知道是否可以直接与FPGA连接?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DS90LV804的 VIH 最低是 2.0 V,VIL 最高是0.8 V
你要看看你2.5V的FPGA的输出电压
600Mbps,10m的话,最好选取带有预加重的LVDS buffer,比如DS25BR100或者DS90LV004。