你好,
如果只是光电信号到MCU(fpga)IO的话,TXSxx,TXBxx都可以吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢回复
是的,电平转换,5V的光电信号转FPGA使用的3.3V信号,还有TI有直接驱动电磁阀、气泵、隔膜泵的IC吗?
可以实现5V到3.3V双向电平转换,但是需要看data rate是否满足您的应用。
另外,TXS,TXB两系列电平转换DC驱动能力很弱,如果需要带载能力强的话,需要使用SN74系列电平转换器件。
驱动电磁阀,气泵的话,可以看下DRV102这类PWM 磁阀驱动器。