Other Parts Discussed in Thread: SN74LVTH244A, SN74LVCH244A
1、在SN74LVTH244A的手册的第一页上有如下表述“Support Mixed-Mode Signal Operation (5-V Input and Output Voltages With 3.3-V VCC)”,应该是说这款芯片可以用3.3V的供电电压可以实现5V电平的输入输出,5V电平输入好理解。这款芯片是采用CMOS技术就不宜采用输出上拉电阻的形式,那怎么实现3.3V供电5V电平输出呢。
2、在不用引脚的处理上,手册第二页有如下表述“Active bus-hold circuitry is provided to hold unused or floating data inputs at a valid logic level. Use of pullup or pulldown resistors with the bus-hold circuitry is not recommended.”,里面的“Active bus-hold circuitry”不用上拉下拉电阻怎么实现呢。