我们现在是自己设计的953板子,接954_EVM板,请问下,如何判断953和954、sensor与953两个通讯的正常?另外,IIC如何通过954/953去写前端的RAW sensor?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通过Processor,读写953和远端sensor的寄存器。看看结果是不是对的
REG = 0x7A, 0x4C, 0x0f
REG = 0x7A, 0x58, 0x58
REG = 0x7A, 0x5C, 0x30
REG = 0x7A, 0x5D, 0x42
远程读写,是这样吗?
关于I2C是如何通过954/93去写前端RAW sensor的问题,建议您参考这篇应用手册,它是以DS90UB913,914为例详细描述了I2C是如何通过主机与远端的SER/DER 以及远端slave(sensor/camera)通讯的:
http://www.ti.com/lit/an/snla222/snla222.pdf
如果有问题,可以随时讨论。
你好 我现在配置OK了 图像也有,但是异常,还请帮忙看下
我的图像格式是1920*1080, 40fps,RAW12, 2-lane MIPI
不好意思才看到,我解决了。修改一个寄存器就好了。你解决没有?主时钟配置要根据你的sensor来设定,如果你确定设置好了,还是这种情况,我可以帮你检查下驱动。邮箱:mengnismd@163.com