usb3.0的设备断掉D+,D-还能正常传输USB3.0的数据吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
USB3.0数据传输用的不是两对高速信号线吗? USB3.0设备的D+、D-是为了兼容2.0设备。
使用的是USB3.0 HUB还是transceiver?像TUSB1310这款transceiver,如果只使用PIPE interface(3.0),2.0的部分不用应该是没问题的。
usb3.0和d+d-可以同时工作么,
即,usb3.0高速连接到一个usb3.0设备,USB2.0信号连接到另外一个USB2.0的设备上面。
把他们当成两个独立的USB口使用,可以么。。